{}

Our Brands

{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What are the Minimum and Maximum mounting depths for Smart-UPS rails?


Issue:

What are the Minimum and Maximum mounting depths for Smart-UPS rack mount rails?

Product Line:

Smart-UPS

Environment:

All rack mounted models, All Serial Numbers
This includes the UPS as well as any associated external battery packs.

Cause:

Smart-UPS Rackmount units (typically designated with "RM" in the part number) include a system of rails and brackets to mount the unit in a typical IT rack enclosure. The rails are adjustable to allow for a range of different sized racks. For specifics of how to mount your unit, please refer to the installation documentation included with your UPS or External Battery Pack.

Resolution:

For all Smart-UPS products 10Kva or less:
The minimum depth for the rails is 21.75" and the maximum depth is 36".
NOTE: If your Smart-UPS is equipped with cleats (metal pieces attached to the sides of the Smart-UPS chassis that slide into the rails) the minimum depth is 29"".

For Smart-UPS products over than 10Kva:
The minimum depth for the rails is 27.5" and the maximum depth is 33".


If you are using your APC rail kit to mount non-APC equipment your experience may vary.
Please note that some networking specific or custom enclosures may need to be adjusted to accommodate the depth of the rails.

Explore more
Explore more

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.