Browse FAQs

PowerChute Network Shutdown VM priority groups explained

Published date: 25 February 2020

Issue:
What are priority groups in PowerChute Network Shutdown?

Product Line:
PowerChute Network Shutdown version 4.3

Environment:
PowerChute Network Shutdown version 4.3 configured with VMware vCenter Server. 

Cause:
Informational

Solution:
Virtual Machines, virtual appliances and the vCenter Server Appliance can be grouped into priority groups - High, Medium, Low, Group 1, Group 2, and any remaining will be un-prioritized. When VM Prioritization is enabled, an inventory view of the datacenter, clusters, VMs and vApps appears on the left. On the right, the High, Medium, Low, Group 1, and Group 2 priority groups are listed.


You can assign a VM/vApp to a priority group by clicking on a VM/vApp on the left-hand side and dragging it to a priority group on the right. You can select multiple VMs/vApps by pressing the CTRL key on the keyboard while clicking on the VMs/vApps you want to move. You can also click on the cluster icon to select all VMs within that cluster, or click the datacenter icon to select all clusters of VMs/vApps within that datacenter.
 
Move VMs/vApps between priority groups by dragging them from one group to another. To remove a VM/vApp from a priority group, select the VM/vApp and click the Remove button. 
Any VM/vApp in the inventory that is not assigned to a priority group is considered to be Un-prioritized.

If as in the example above the High priority group has a delay set to zero any powered on VMs/vApps that are included High priority group will be skipped. The High priority VMs/vApps will remain powered on. This may be helpful when working with VMs/vApps that need to remain running after the vCenter Server VM is shut down e.g. Storage or Controller VMs. If these VMs/vApps require graceful shutdown, then an external script can be configured via the Shutdown Command file feature in PowerChute to do this. Please note that these VMs/vApps that will not be powered up automatically by PowerChute if VM Startup has been enabled. 

NOTE: Setting any priority group with a zero second delay for Migration, Shutdown, and Startup will have the same affect.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.