Video: How to change the Maintenance Intervals on a Network Air FM unit
Published date:
16 October 2019
Issue:
This document contains a video on how to change the Maintenance Intervals on a Network Air FM unit.
Product line:
FM35-50, ACFM, IR40.
Environment:
All Serial Numbers.
Cause:
Install Operation.
Resolution:
How to change the Maintenance Intervals on a Network Air FM unit follow the below procedures.
1 Press ESC until you reach the main menu (On/Off).
2 Scroll to SETUP and press ENTER.
3 Scroll to SYSTEM 1 and press ENTER.
4 Press ENTER on ALARMS.
5 Press ENTER on MAINT ALARMS.
6 Press ENTER to scroll through the device available.
1 of 7 Compressors 1
2of 7 Compressor 2
3 of 7 Heaters
4 of 7 Blowers 1
5 of 7 Blowers 2
6 of 7 VFD 1
7 of 7 VFD 2
7 Press ENTER on the selected device.
8 Press the DOWN arrow once then press ENTER again.
9 Using the UP or DOWN arrows you can select the desired interval or disable this feature.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.