Changing the DNS hostname on a Uniflair with a touch screen display.
Published date:
17 July 2020
Issue:
This document describes how to change the DNS Host Name on a Uniflair with a touch screen display..
Product line:
Uniflair PCO5.
Environment:
Data Center Cooling.
Cause:
Resolution:
When changing the host name manually for the DNS server in the network interface on the unit, the name needs to be formatted as xxxx.x to be accepted. The preceding xxxx can be a combination of letters and numbers but the .x must be a letter or letters. Examples are .com, .net, .edu, .ca, .sdf, .f, .h ect. The interface will show the following error if this naming convention is not followed.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.