Is there a roof fan available for the NetShelter SV cabinets?
Published date:
05 August 2019
Issue:
There does not appear to be an optional roof fan for the NetShelter SV cabinets.
Product Line:
NetShelter SV
Environment:
All versions and serial ranges.
Cause:
A request has been made to add a roof fan to a NetShelter SV.
Resolution:
The NetShelter SV cabinets do not currently have roof fans available.
Some of the fans that can be used inside the SV cabinet are: ACF001, ACF002, ACF003, ACAC40001, ACF201BLK, ACF202BLK.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.