Uniflair BACnet (Building Automation and Control Networks)
Published date:
18 July 2020
Issue:
This document describes the operation of the Uniflair BACnet (Building Automation and Control Networks).
Product line:
Uniflair
Environment:
All Models and Serial Numbers
Cause:
Install
Resolution:
All the units must be fitted with a RS485 card, trough that they are connected to the RS485 serial cable. On one side there will be the 120 ohm resistor, on the other, the gateway which will translate the variables from Uniflair language, to LON language.
To realize a local net to be connected to a BMS with protocol BACnet, it’s necessary:
• gateway LBM every 8 units; (not necessary with pCOnet - pCOWeb)
• 1 RS485 serial card for every controller;
• 120Ω resistor;
• PC for the gateway configuration
BACnet is a supervisory system created from AHRAE:
“American society of Heating, refrigerating and Air conditioning Engineers”
These are the ways how the information under BACnet can be sent to Uniflair controllers:
BACnet IP/Ethernet
pCOnet:connessione RS485
Gateway
Carel :
Protocol Carel
Connection RS485 or RS422
Max 8 units
No software modification needed
BACnet :
BACnet PTP
Connection RS232
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.