Are there baying brackets available for the NetShelter VX Seismic cabinets?
Published date:
20 February 2020
Issue:
A question is asked ifit's possible to bay together NetShelter VX Seismic cabinets.
Product Line:
NetShelter VX Seismic
Environment:
All versions and date ranges.
Cause:
Customers may want to use baying brackets to enhance the seismic feature, or to help align rows of cabinets.
Resolution:
There are no baying brackets for the NetShelter VX Seismic cabinets.
The NetShelter VX Seismic cabinets are designed to be mounted to the floor in NEBS GR-63-CORE seismic installations, and baying brackets are not necessary. Baying brackets do not enhance the seismic feature of the cabinet.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.