Power Over Ethernet configuration supported by NetBotz products.
Published date:
22 July 2020
Issue:
Power Over Ethernet configuration supported by NetBotz products
Product Line:
NetBotz
Environment:
NetBotz version 3 Rack appliances and POE
Cause:
POE options that work with supported NetBotz version 3 rack appliances.
Resolution:
IEEE compliance offers 2 alternatives for Power Over Ethernet (POE). Alternative 'A' allows for power to be passed through wires 1, 2, 3, and 6 on a Cat-5 switch are the transmit and receive wires. Alternative 'B' allows for power to be passed using the unused pairs 4, 5, 7, and 8 on a Cat-5 cable.
Alternative 'A' is usually output by a switch or endspan device. Alternative 'B' is more often used by a midspan device such as a POE injector. APC's POE injector (NBAC0303) inserts power on the Cat-5 cable using alternative 'B'
NetBotz POE compatible appliances work with either alternative and should power on with alternative 'A' or 'B'.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.