Once the I/O Device is connected to the Appliance, configuration for the Seal/O device can be done by the following:
1. Launch the Advanced View on the Appliance.
2. Double click the 'Serial Devices' Applet
3. In the drop-down menu, select the Sea-Level Product >> SeaLevel SeaI/O 450.
4. Then select 'OK'
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.