Технические часто задаваемые вопросы



Can depth extenders such as ACDC2551 be added to the rear of a 1200mm deep cabinet?
See page 17 of the attached file "NetShelter ATO Custom Cabinet ... this link: http://www. apc .com/ ...
How accurate is the current monitor on my APC Rack Power Distribution Unit (PDU) and Rack Automatic Transfer Switch ?
are tested at a current load of 17 .5 amps at Crest Factor of 3.0 to Outlet #1 (phase L ...
APC KVM Switches and Corresponding Cables/Server Modules
APC KVM Part Numbers and Corresponding Cables/Server Modules ap5808 - 17 " Rack LCD Console with Integrated 8 Port Analog KVM Switch
Data Center Expert | Alarm "Device status may be inaccurate due to attempt to transfer DDF failed"
APC Networked Devices APC Network Management Card ... ... the discovery of APC devices and after ... update of an APC NMC, Data ... Checking APC NMC log files ... ... interface of the APC NMC using administrator ... ... /SCP on APC NMC. ... /SCP on APC NMC ... interface of the APC NMC using administrator ... ... interface of the APC NMC using administrator ... ... interface of the APC NMC using administrator ... ... interface of the APC NMC using administrator ... ... settings from the APC NMC. Note ... ... .10. 17 .1- ... .10- 17 .* This firmware is available for download on the APC web site as well as in the newest StruxureWare DCE firmware catalog.
How to roll back NetBotz firmware.
www. apc .com/tools/download ... Please note that when downgrading, it is suggested that you not keep any of the old configuration and do not use the "rootupgkeep" option in step 17 .
NetBotz TFTP upgrade/recovery procedure
1) Download the most recent firmware from apc .com for your NetBotz Appliance (355, 455, 450, 550, or 570). ... 17 ) Issue the following command: rootupg <enter> This process will take approximately 7-8 minutes to complete. ... Log into the appliance using a username/password of root/ apc to set the new root password and network settings on the appliance.


Результаты 1 - 10 of 52

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.