Creating an Aggregate Device within the KVM Access Software
... case of utilizing Rack PDU Power Integration ... ... device effectively creating 150 nodes in total ... 5 .) Optional: ... The choices are Generic, Dell DRAC 5 , Dell iDRAC 6, HP ilo2, and IBM RSAII. ... Options are IPMI, Dell DRAC 5 , Dell iDRAC 6, HP ilo2, or IBM RSA II. ... 5 .) When you return to the Port List page, the selected ports are automatically unlocked and are listed as being associated with the Aggregate Device.