DAC, Cancoil Installation Manual
... ….. 5 ... ….. 5 Section 5 . Start Up ... ….. 5 ... and electrical and capacity data, please ... ... designed to provide years of reliable performance ... stable, efficient year round operation for ... Suction riser capacity is the MINIMUM ... System Capacity . ... a pressure of 250 microns. Section 5 . Start- ... ... system must be adjusted at start- ... ... in response to changes in the outdoor ... ... thermostats should be adjusted according to the ... The condenser capacity is reduced and the head pressure rises. During periods of warm outdoor temperature, the liquid returns to the refrigerant receiver, and the condenser returns to full capacity .