Browse FAQs

How can I check the battery voltage of my XBP48RM1U-LI / XBP48RM1U2-LI?

Published date: 26 November 2019

The XBP48RM1U-LI and XBP48RM1U2-LI have battery management electronics in them, and when the battery pack is unplugged from the UPS this is sensed and the battery pack output is turned off. This means we cannot measure the battery voltage from the cable unlike the external battery packs with VRLA Batteries.

To check the battery voltage either
  • First remove AC power from the UPS
  • On the Display choose Status
  • Choose Battery
  • Scroll to page 5 to see the battery voltage (as the AC power is removed this will just show the battery voltage rather than the charging voltage)
Or
  • First remove AC Power from the UPS
  • Measure the voltage on the Battery Pack Anderson socket with a voltmeter (as AC power is removed this will just show the battery voltage rather than the charging voltage)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.