Internet Explorer downloads NetBotz 5.1 upgrade as a .ZIP file
Published date:
20 May 2020
Issue:
Internet Explorer downloads NetBotz 5.1 upgrade as a .ZIP file
Product Line:
NetBotz
Environment:
NetBotz Upgrade File
Internet Explorer
Cause:
Internet Explorer 11 (and possibly other versions) see that the "PROD_SIGNED_NBRK0750_Build_5.1.0.31.sedp" NetBotz upgrade file is a compressed file and IE renames it to a .zip file
Resolution:
Either use a different browser such as Google Chrome or in IE, choose to "Save As" and rename the file from a .zip extension to a .sedp extension before saving. This can also be done after the file is downloaded.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.