Video: How do I change the temperature units within the StruxureWare Data Center Expert Client?
Published date:
12 September 2020
Issue:
How do I change the temperature units within the StruxureWare Data Center Expert Client?
Product Line:
StruxureWare Data Center Expert
StruxureWare Central
Environment:
StruxureWare Data Center Expert all versions
Cause:
The StruxureWare Data Center Expert client temperature units are configured based on the formats setting of the workstation running the client.
Resolution:
The StruxureWare Data Center Expert client temperature units are configured based on the formats setting of the workstation running the client. To be able to manipulate temperature units within the client the workstation "Formats" settings must reflect a format with displays the correct units. This artical explains how to change the clients from either Fahrenheit to celsius or vise versa within Windows 7 workstation.
Changing the client from Fahrenheit to celsius
1. Close the current session of the Data Center Expert client
2. Click on the "Start" icon. This is tradionaly located in the bottom left of the GUI
3. Click on "Control Panel"
4. Click on "Region and Language"
5. Click on the "Formats" tab
6. Under the "Format" drop down select English (United Kingdom)
7. Click OK
8. Reopen your Data Center Expert client
Changing the client from celsius to Fahrenheit
1. Close the current session of the Data Center Expert client
2. Click on the "Start" icon. This is tradionaly located in the bottom left of the GUI
3. Click on "Control Panel"
4. Click on "Region and Language"
5. Click on the "Formats" tab
6. Under the "Format" drop down select English (United States)
7. Click OK
8. Reopen your Data Center Expert client
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.