Resolution:
Please call tech support at 1-888-695-6500 and hit option to three times to get to the cooling team to verify part numbers before ordering, as they may change.
ACF400 break down
This is the entire fan and power system.
ACF115 APC Rack Air Removal Unit SX Fan Assembly 100-240V 50/60 Hz (All 4 fans and Electronics module included)
ACF136 APC Rack Air Removal Unit SX 600mm Wide Frame
ACF126 Ducting Kit
W0M-7053 ASSY ARU GEN 2 ELECTRONICS MOD
W0M-7054 AIR REMOVAL UNIT G2 REPLACEMENT FAN MODULE
0J-0G-9233 GENERIC ANSI WWPV LCD DISPLAY
0J-0W2818A Temperature Sensor (Optional)
AP9324 Beacon (Optional)
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.