Browse FAQs

Which accessories/environmental sensors are compatible with my APC Network Management Card (or devices with embedded Network Management Cards)?

Published date: 22 January 2021


Issue

Which accessories or environmental sensors are compatible with my Network Management Card (or devices with embedded Network Management Cards)?


Product Line
 

  • Network Management Card 1 - AP9617, AP9618, AP9619

Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches.

  • Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/35CH

Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Rack Automatic Transfer Switches (AP44XX), Smart-UPS Online (with model prefix SRT).

  • Network Management Card 3 - AP9640, AP9641
 
Environment
 
  • All serial numbers
  • All installation scenarios
  • All firmware versions (unless otherwise noted)
  • Compatibility excludes NetBotz devices


Cause

General compatibility information relating to supported accessories that can be connected to the "Sensor" or "Universal Input/Output (UIO)" ports. Please note, compatibility excludes NetBotz branded items that contain an onboard Network Management Card, such as NetBotz 200. Please refer to NetBotz sensor compatibility information.



Resolution

Refer to the table below - our newest products and offers are located at the top of the table. 
 
 
Device/Available UIO Ports Quantity of Accessory Ports/Type Firmware Application Name Accessories/Sensors Supported
AP9640 0 Any
  • N/A, no Universal Input/Output port(s) available
AP9641 2/UIO Any
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
AP9630 or AP9630CH 0 Any
  • N/A, no Universal Input/Output port(s)available
AP9631 or AP9631CH 2/UIO Any
  •  
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
AP9635 or AP9635CH 1/UIO Any, sypx - v5.1.3 or higher required
  • AP9335T Temperature Sensor
  • AP9335TH Temperature and Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
Smart-UPS Online (with model pre-fix SRT, available mid-late 2014) 1, integrated UIO sumx
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
AP8XXX series Rack PDU 1/UIO
1/RJ-12 Serial
rpdu2g
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • RJ-12 Serial Port only: RF Code (Third Party) R170 Sensor Tag, requires rpdu2g v6.0.9 and higher
AP44XX Rack ATS 0 ats4g
  • N/A, no Sensor port(s) available
AP9617 0 Any
  • N/A, no Sensor port(s) available
AP9618, AP9619 1/Sensor Any
  • AP9512T or AP9512TBLK
  • AP9512TH or AP9512THBLK
AP77XX Rack ATS 0 ats, g2ats
  • N/A, no Sensor port(s) available
AP7XXX series Rack PDU 0 rpdu
  • N/A, no Sensor port(s) available
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.