Browse FAQs

Why doesn't the serial communications work on a Smart-UPS SUA model when USB communications has been tried first?

Published date: 14 January 2020


Issue:

Connecting a USB cable to an SUA Smart-UPS disables the serial port
  
Product Line:

Smart-UPS

Environment:

All SUA models, All Serial Numbers

Cause:

Normal operation.

Resolution:
In order to regain serial communications with an SUA model Smart-UPS after USB has been used, the USB cable must be removed and the Smart-UPS must be brain deaded. To brain dead a Smart-UPS, the load must be turned off and unplugged. Next, the UPS must be turned off and unplugged. Once unplugged, push and hold the off button for 6 to 8 seconds. The sensitivity light in the back of the UPS should go out and there should be a small audible click in the unit. Serial communications should be enabled at this point and the UPS can be again plugged in and started up.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.