Pesquisar Perguntas frequentes



Are 23" mounting rails available for NetShelter SX cabinets?
All 42U and 48U NetShelter SX 750 mm (30") wide cabinets are available with 23" mounting rails installed.
ACSC1XX Spare Parts List
BAYING BRACKET NETSHELTER SX ... (2.3 FEET (700 MM ) LONG) ... DC RECTIFIER, 500 WATT, 54VDC, WIDE INPUT, FULL SIGNALS, BLACK ... LATCH FLUSH SLAM W/ TUMBLER #333 (for side door panels) ... 750 -0034
What is the exact placement of the cutouts on NetShelter SX mounting rails?
... , hole, holes, pma, 42u, 45u, 48u, 600 mm , 750 mm , 600mm, 750mm,
Can the horizontal cable side channel organizer be installed into a 600mm wide NetShelter SX, VX or SV cabinet?
Issue: The ar8008blk and ar8016ablk are designed to install into the mounting rails of NetShelter SX 750mm wide cabinets.
Will the NetShelter CX fit through standard doors?
They measure 750 mm /29.5” wide x max 1950mm/76.7” tall.
Can the NetShelter SX cabinets be bayed with the side panels on, and how do the baying brackets work?
NetShelter SX ... NetShelter SX cabinets are designed to be bayed together with the side panels in place. Every NetShelter SX cabinet ships with the required baying hardware included eliminating the need to order multiple part numbers to compete a row. The design of the NetShelter SX baying hardware allows for a single cabinet with equipment installed to be removed from a row. ... Simply loosen the bracket and rotate it to the side . ... There are two alignment holes on the bracket allowing the cabinets to be joined at 600 mm on center, or 24 inch on center.
What width cable ladder will attach to the pass-through data cable partitions?
Customers need to choose the correct width cable ladder when attaching to a pass-through data cable partition. ... NetShelter SX Ladder and Partitions ... It appears that there is only one set of cable ladder attachment holes on the side of the pass-through data cable partition. ... The holes of the pass-through data cable partition were expanded and only the 12" wide cable ladder will attach to it.
InfraStruXure™ InRow Data Cable Bridge Partition, 300 mm Wide—acac10005
Issue: This document describes how to install a InfraStruXure™ InRow Data Cable Bridge Partition, 300 mm Wide —acac10005.
How to install InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide—acac100010
Issue: InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide —acac100010.


Resultados 1 - 10 de 79

Não encontra o que procura?

Contacte a nossa equipa de apoio ao cliente para receber informações sobre assistência técnica, assistência relativamente a reclamações e muito mais.