Consultar las preguntas frecuentes



Why can't I use a domestic model APC UPS on a ship
Issue: In North America, one would expect to see approximately 120 volts when
What is AVR (Automatic Voltage Regulation)?
Product Line: Line-R, Back-UPS, Back-UPS PRO, Smart- UPS and APC AV.
Frequently Asked Questions for the new SMX and SMT series of Smart-UPS products.
... of Smart- UPS products. Smart- UPS SMT and SMX ... of Smart- UPS is an all ... of Smart- UPS product with many ... UPS Frequently Asked Questions APC’s patent pending ‘ ... that perform automatic voltage regulation ( AVR ) when not ... AVR is typically handled ... ... do the new UPS’s not have a ... ... addition to a USB port and both ... New Smart- UPS models utilize PowerChute Business Edition version 8.5 or later only. ... We recognize the fact that some Smart- UPS customers utilize their own custom interface based on APC’s UPSLINK protocol. ... UPS UPS UPS ... UPS
Video: Why might my APC Back-UPS Product be beeping?
APC's UPS Selector ... indicates that the UPS has detected an ... ... determine if your UPS is capable of ... 5 .) Disabling UPS audible alarm tones ... ... software, the UPS audible alarm tones ... ... 1 beep every 5 seconds ... If the input voltage is determined to ... equipment, the UPS will transfer to ... ... for the acceptable voltage window. The UPS is trying to ... ... unit shipped with APC management software it ... the default acceptable voltages that the unit ... ... section of the APC management software for ... ... + or - 5 % this will ... ... is 3 to 5 times the size ...
Where can I get support for APC and MGE Products?
... M 12000- 5 M 12008- ... M 12008- 5 M 12012- ... 5 M-E ... E 12032- 5 M 12032- 5 M-E ... M 12037- 5 M 12084- ... ... M 12084- 5 M 12137- ... M 12137- 5 M 12143- ... M 12143- 5 M 12145- ... E 12145- 5 M 12145- 5 M-E ... ... M 12147- 5 M 12148- ... M 12148- 5 M 12215- ... M 12215- 5 M 1423- ...
Why might the LEDs on my Back-UPS or Smart-UPS SC be flashing?
... -UPS Pro USB , Back- ... and Smart- UPS SC: causes ... ... Back-UPS USB , Back- ... , Smart- UPS SC 620va and ... ... in troubleshooting your UPS , please access ... ... indicates that the UPS is performing a ... ... indicates that the UPS has entered " ... " where the UPS will turn off ... The UPS is put into ... ... Guide) your ups may "" ... ... "" your UPS , press the ... ... indicates that the UPS is operating normally ... ... indicates that your UPS is operating on ... The UPS can only provide ... If your UPS is operating on ...
How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: ... firmware of the UPS : ... a Serial or USB connection using the ... ... All Smart- UPS via USB or Serial communication ... ... below Smart- UPS devices: ... smx1500 with firmware UPS 02.x ... ... These units are 120 V devices built ... ... find your current UPS Firmware version via UPS LCD: ... menu of the UPS LCD screen, ... down to " UPS Firmware". ... find your current UPS Firmware version via ... ... find your current UPS ID: ... Every Smart- UPS has a unique UPS ID. ... menu on the UPS LCD screen, ...
Can I use a domestic model UPS in a foreign country?
APC's North American units ... an input requirement of 120 volts , 50-60hz and an output of 120 volts , 50-60hz.
No serial communications on SUA Smart-UPS after connecting USB Cable
Now hold the off button in for 5 to 10 seconds until you hear ... sensitivity LED in the back of the UPS goes out .
Video: What are the basic troubleshooting steps for the Back-UPS ES model be600m1, bn650m1/bn650m1-CA/BN675M1?
APC Back-UPS ... ... may find your UPS not functioning as ... ... brownout or over voltage condition. Contact APC Technical Support for ... Leave the Back- ... ... tone and the UPS is off • The UPS was on battery ... load of the UPS . Turn off the UPS . ... Turn on the UPS and reconnect the ... USB charging is slow ... device using the UPS's USB charger is slower ... the device's original USB charger The amount ... compatibility with the USB Battery Charging Specification ... USB charging stops and ... The USB ports has detected ... ... device from the USB port. USB charging will resume ...


Resultados 1 - 10 de 74

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.