FAQ techniczne

Zadaj pytanie

Filtruj wyniki

    What Proximity Cards are supported by the NetBotz NBACS125 & NBACS1356 Rack Access Control Systems?
    Additional packs of 10 cards (ap9370- 10 ) can by purchased from APC by Schneider Electric.
    Is there a limit to the number of e-mail addresses that can be configured to receive alerts from a NetBotz device?
    ... alerts from a NetBotz device? NetBotz NetBotz version 2 and ... ... a primary, secondary , or short ... ... that makes a NetBotz appliance extremely versatile ... ... also cause the system to get bogged ... It is suggested that if more than 10 recipients need to be e-mailed about a specific alert that an e-mail group be created in your SMTP server. This way, the NetBotz appliance can be configured to send a single e-mail to this group and in turn, hundreds of recipients can be configured to receive an e-mail.
    NetBotz TFTP upgrade procedure.
    NetBotz TFTP upgrade procedure ... NetBotz version 3 NetBotz model: 355 ... Optional NetBotz firmware upgrade/ ... ... for restoring a NetBotz appliance to default ... behavior on a NetBotz appliance. ... segment as the NetBotz Appliance. ... plugged into the NetBotz Appliance during this ... ... the for the NetBotz Appliance. ... traffic between the NetBotz Appliance and the ... ... power from the NetBotz Appliance while keeping ... 10 ) You should ... be at a NetBotz > prompt. ... address for the NetBotz Appliance) ... address for the NetBotz Appliance) ... mask for the NetBotz Appliance) ... (reboots the NetBotz Appliance)
    NetBotz 750 | Physical Description
    ... Description of the NetBotz 750 NetBotz version 5 NetBotz v5. ... ... a maximum of 10 A. Activates ... ... for connecting a NetBotz Leak Rope Sensor ... ... sensors require the NetBotz Dry Contact Cable ... sensors require the NetBotz 0-5 ... 8 10 /100/1000 Network Port Provides a connection to the network. ... See for additional information. 9 Private LAN Provides a 10 /100/1000 connection to a private local area network and 48 VDC to an attached device. 10 Wireless Sensor Coordinator USB Port with Wireless NetBotz USB Coordinator (nbwc100u) installed.
    Why does the NetBotz wireless device LED stay red.
    NetBotz wireless device LED stays red. ... NetBotz version 3 ... NetBotz wireless sensors / pods nbsp180 ... When you do a long reset button push the led goes red after 10s of holding the button in and if the button is physically stuck in the red led will stay on. ... You can clear the LED by freeing the button. To free the buton, move it around or side to side using a pin or paper clip.
    Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X
    ... with version 3 NetBotz and BotzWare 4 ... NetBotz NetBotz nbwl0455 and nbrk0570 ... been tested with NetBotz 4.0 ... ... note that the NetBotz 3xx and NetBotz nbrk0450/0451 ... With the release of Botzware 4.2, the following list of additional Pelco cameras and firmwares have also been tested: ... IL 10 Sarix Unavailable ... Pelco Sarix Pro models that were originally listed as supported do not correctly update the resolution settings presented to NetBotz appliances. NetBotz can no longer support Sarix Pro models due to this limitation of the Pelco camera and they have been removed from this compatibility matrix.
    Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
    ... ,8 and 10 KVA FAQ ... SRC 5- 10 KVA UXI Models ... Q: What is the use of Parallel Kit (srcpk001 & srcpk002)? ... A: The Parallel Kit allows you to connect the two UPSs' output supply to the load via a common AC bus bar. ... Q: What are the advantages of the SRC 5- 10 KVA LCD Display? ... A: In addition to the 1+1 Parallel redundancy system , the Customer can also look into a service bypass panel which will give you a wrap around bypass.
    Where can I get support for APC and MGE Products?
    Additional Management Cards and Options ... Air Distribution Accessories ... AIS Accessories AIS Battery Systems ... AV Accessories ... Back-UPS Accessories ... Configurable Power Accessories ... Data Center Software Integration Kits ... Environmental Management System ... Hardwire Surge Suppression Accessories ... Matrix Battery Systems ... Matrix-UPS Accessories ... MGE Accessories ... MGE Battery Systems ... Modular Power Accessories ... NetBotz 200 NetBotz 300 NetBotz 400 NetBotz 500 NetBotz Access Control NetBotz Accessories and Cables NetBotz Central NetBotz Rack Access NetBotz Sensors ... NetShelter Open Frame Rack Accessories ... NetworkAIR Accessories ... Power Generation Systems ... Rack PDU Accessories ... Room Cooling Accessories ... Row Cooling Accessories ... Silcon Accessories Silcon Battery Systems ... Smart-UPS Accessories Smart-UPS Battery Systems ... Software for NetBotz Appliances ... Spare Part Kits ... Symmetra Accessories Symmetra Battery Systems ... Symmetra MW Accessories ... Symmetra PX Accessories ... TSP Accessories ... TSP/Total System Power ... Universal Power Accessories
    What type of information is provided in an SNMP trap from StruxureWare Data Center Expert?
    .iso.org.dod.internet.private.enterprises.netBotzAPC. netBotz .netBotzTraps .1.3.6.1.4.1.5528.100. 10 ... If you are using the "Network Management Systems Integration" feature, these traps are sent using the powernet mib. ... The traps also provide additional information / arguments as described in the mib:
    Video: Network Management Card (NMC) Password Reset Procedure
    ... , ap9340, Netbotz 200) In addition , if you ... than one SmartSlot accessory installed in it ... the other SmartSlot accessories to gain direct ... ... Please reference that accessory's user guide on ... ... sure that the accessories are installed in ... ... -9) Netbotz 200/Environmental ... ... no flow control Netbotz 200/Environmental ... From the Control Console menu, select System , then User Manager. ... 10 .) ... In addition to possibly neededing to reset its password, you may need to re-enable the account if no other administrative access is available or known.