Browse FAQs

PMM 400 - PMM 500; Modbus RTU 4-Wiring to NMC interface board

Published date: 22 July 2020

Issue:
Modbus RTU 4-Wiring to NMC interface board


Product line:
PMM 400 / PMM 500


Environment:
PMM 400 / PMM 500


Cause:
Customer wants to connect to the NMC interface board instead of Modbus RS45 connector on the outside of the communication box.  The installation/operation manual does not give details on how to connect 4-wire to the NMC interface board.


Resolution:
See wiring diagram below.
 



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.