Browse FAQs

Why is the Galaxy VX 10-inch display alarming when ODBX breaker is closed instead of alarming in an open state?

Published date: 15 July 2020

Issue:
10-inch display alarming when ODBX breaker is closed instead of alarming in an open state


Product line:
Parallel Galaxy VX with Magelis 10-inch display.


Environment:
All Galaxy VX Magelis 10-Inch Displays.


Cause:
Incomplete configuration


Resolution:
Access the “Configuration” screen then the “Customer” screen then “Output Setup” and change the “Normal State” to Open for the breakers in question and click on OK button to complete the configuration.




 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.