Browse FAQs

Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?

Published date: 15 July 2020

Issue:

Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?


Product Line:

NetBotz


Environment:

NetBotz cameras


Cause:

NetBotz has released the NBPD0165 camera pod.


Resolution:

No, the camera pod NBPD0165 is not compatible with NetBots 3xx, 4xx, and 5xx devices. There are currently no plans to integrate the cameras into the older appliances. As of it's release, it is only compatible with the NetBotz 750 series appliances.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.