Technical FAQs

Ask a Question

How to make sure the IT equipment's mounting rails will install into a NetShelter cabinet after moving the mounting rails in for cable management.

Issue:
IT equipment comes with mounting rails. All mounting rails have minimum and maximum mounting depths. 

Product Line:
NetSheltetr SX 

Environment:
All versions and serial ranges.

Cause:
Adding cable management and PDU/accessory mounting rails to a cabinet require the mounting rails to be moved inward. 
Since the equipment's mounting rails have a min/max depth specification, at some point it's possible to move the rails inward enough that the equipment will require a short-depth monting rail. 
Understanding this ahead of time allows the customer to either move to a deeper cabinet, or order the correct rails. This will help avoid delays. 
This issue is most likely to occur with standard depth cabinets, but can also occur in deeper cabinets. 

Resolution:

See attached file. 
 
Was this helpful?
What can we do to improve the information ?