Browse FAQs

What is the NetBotz smoke sensor NBES0307 sensitivity?

Published date: 16 July 2020

Issue:

What is the NetBotz smoke sensor sensitivity?

Product Line:

NetBotz sensors

Environment:

NetBotz smoke sensor NBES0307

Cause:

Customer request for sensor sensitivity.

Resolution:

The nominal detection sensitivity for the NBES0307 is 2.5 percent-obscuration-per-foot. This is not configurable on the sensor and the NetBotz appliance will only see the sensor as a state sensor...smoke or no smoke. A variable threshold (such as those available for a numeric sensor such as temperature) is not possible.

Please see the attached datasheet for more smoke sensor information. Please see the NetBotz product page for more recent documentation.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.