Browse FAQs

Video: How to place an ACRD200 unit into Standby or On

Published date: 18 July 2020

Issue:
How to put an ACRD200 unit into On or Standby.

Product line: 
InRow Cooling Products ACRD200.

Environment:
All Serial Numbers.

Cause:
Install, Configuration.

Resolution:
 


First you need to access the On/Standby menu
 
Then select ENTER
 
You will be prompted for a Password if limited access is enabled
 
Use the default password of “apc”
 
If this does not work check with your Admin for the correct password
 
If password has been lost use the last eight digits of the serial number
 
Now you should be able to choose either On or Standby
 
Press ESC and now you should be able to change Limited access from No to Yes
 
Limited access set to yes will only allow users to turn unit On or Standby with correct password.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.