Browse FAQs

How to check the model and serial number of an ACRP500

Published date: 18 July 2020

Issue:
This document explains how to check the model and serial number of an ACRP500.
 
Product line:
ACRP500.
 
Environment:
All serial numbers.
 
Cause:
To help tech support identify the unit and its warranty status.
 
Resolution:
 
Press the < ESC> button until you get to the “ON/STANDBY” screen. Then use the down arrow to scroll though the display. When you get to the screen “ABOUT INROW” stop and make sure the arrow on the left side of the display is pointing at it and the hit the <ENTER/RETURN> button.
 
Now you have access to:
 
MODEL
 
SERIAL NUMBER
 
FIRMWARE
 
HARDWARE
 
MFG DATE
 
APP
 
AOS VERSION


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.