Browse FAQs

Netbotz | How to generate a new SSL Certificate

Published date: 15 July 2020

Issue:
How to generate a new SSL Certificate

Product Line:
NetBotz

Environment:
NetBotz using SSL communications

Cause:
The SSL Certificate date is generated based on date and time settings of appliance. When these values are set incorrectly when initial SSL certificate is being generated the only way to change it is to generate new certificate. This can be used for any SSL issue that may require the cert to be recreated.

Resolution:
In order to do those make sure the date is properly set and then change the hostname, a new certificate will be automatically generated with correct values. The hostname can then be reset to the original if necessary.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.