Browse FAQs

Netbotz SP155 readings are inaccurate

Published date: 17 July 2020

Issue:

Netbotz SP155 readings are inaccurate with version 3.0.0 Botzware.

Product Line:

NetBotz

Environment:

Netbotz SP155

Cause:

Firmware issue

Resolution:

Upgrading to Botzware version 3.0.1 from version 3.0.0 should resolve any discrepancy in the readings of the SP155. This can be done through the Netbotz advanced view or through InfraStruXure Central.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.