Browse FAQs

NetBotz | Configuring SeaLevel 450 Relay I/O Device

Published date: 28 July 2020

Issue:
Configuring SeaLevel 450 Relay I/O Device within Netbotz

Product Line:
NetBotz v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)

Environment:
NetBotz version 2 and 3
Sealevel 450

Cause:
3rd party device configuration.

Resolution:

Once the I/O Device is connected to the Appliance, configuration for the Seal/O device can be done by the following:

1. Launch the Advanced View on the Appliance.
2. Double click the 'Serial Devices' Applet
3. In the drop-down menu, select the Sea-Level Product >> SeaLevel SeaI/O 450.
4. Then select 'OK'

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.