Consultar las preguntas frecuentes

Do we offer roof fans for 1200 mm deep cabinets? If not, why not?

Fecha de publicación: 19 September 2019

Issue:
Is there a roof fan for the 1200 mm deep cabinets? 

Product Line:
NetShelter SX

Environment: 
All versions and serial ranges.

Cause:
There is a request for a roof fan on a deep cabinet. 

Resolution:
We do not currently offer a roof fan for the 1200 mm deep cabinets. If a customer requires a 1200 mm deep roof fan we can process a custom request. Please contact Sales and advise the quantity needed and required ship date. 
The roof fans are offered for 1070 mm cabinets primarily because, when loaded with cabling, PDUs, etc, air flow can become a challenge. The fan tray helps to alleviate that issue. Similarly, adding space in the back by moving to a deeper cabinet tends to accomplish the same thing. 

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.