Consultar las preguntas frecuentes

General functions of a DG5.0 control platform

Fecha de publicación: 11 June 2016

Issue:
General functions of a DG5.0 control platform
Product line:
Airflow
Environment:
Data Center Cooling
Cause:
 
Resolution:
MANUALLY ROTATE UNITS IN REDUNDANT UNIT GROUP using the following path in the unit addresses as the 1 unit:
Path: Config >> Enter >> Enter (curser at Custom Setup) >> Down Arrow >> Scroll to Page 21 >> Special

TOGGLE THROUGH UNITS IN A SHARED DISPLAY SETUP:
Path: Help and Network buttons at the same time

RESETTING/RECONFIGURING DG5.0 BOARD:
Path: Blank Button >> enter (curser will move to the model above Software) >> Temp. and Run Hours at the same time (curser will move below the Software Ver. # >> Down arrow >> enter
 
BACK DOOR PASSWORD:
Path: Blank button >> Network and Temp at the same time >> Down arrow >> this will take you to the section where you can view or alter the 2 level passwords
 
FACTORY MENU:
Path: Blank button >> Config. >> Enter >> Enter (Curser should be at the Custom Setup) >> Press Special and Config at the same time >> Hit the Down Arrow Key 

CLEARING ALARM HISTORY:
Path: Alarm History >> Blank Button >> Help
 
ADDRESSING THE BOARD to the DISPLAY:
Path: Temp & Humid & Run Hours simultaneously

RESETTING THE CONTROLLER
- Press Blank => Press Enter => Press Temp. & Run hours at the same time … the cursor will move below Software Revision#=> Press UP/DOWN arrow => Press Enter >> Press Enter -Waiting to Reset msg … when the Config screen comes up choose the AC Unit >> Press Enter and scroll through the I/O Setup until the screen reads Cycle Power >> Please cycle power at the breaker of the unit

INSTALLING A NEW BOARD AND SETTING UP UNIT ADDRESS
-          Set dipswitches on the board for the Display and the Clock Card (settings can be found in the manual)
-          Power on the unit
-          Hold down Temp, Run hours, and Humid at the same time
-          Configure the I/O Board to the terminal address
-              NOTE: if nothing shows up use the UP/DOWN to toggle
-          Press enter to access P:01 – terminal 1 (ONE) should read according to dip switch settings which is found in the manual
-          Set the unit according to Pr. (Private) or (Shared)
-          Accept changes to Yes
-          Reset the board
-          Press Blank Red Button =>  Enter (you will see the cursor move to the Model)
-          Press Temp and Run Hours at the same time and the cursor will move below Software Revision#
-          Press the UP/DOWN arrow
-          Press Enter <Waiting to Reset msg>
-          When the Config screen comes up choose the AC Unit
-          Press Enter and scroll through the I/O Setup until the screen reads Cycle Power. 
-          Please cycle power at the breaker of the unit
 

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.