Consultar las preguntas frecuentes



Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... PDU, AV unit , or environmental monitoring unit with an embedded ... ... : Environmental Monitoring Unit 1 (AP9312TH ... ... , Environmental Monitoring Units (ap9320, ... ... , Smart- UPS Online (SRT ... ... device from v 5 . X . X to v6. X . X , please review ... Begin by determining what ... ... in a Symmetra PX 250/500 ... ... installed in a UPS , you need to determine which UPS you have. ... offers several different UPS families. Smart UPS ... phase (Symmetra PX ) Symmetra PX 250/500kva
Dry Contact I/O Options FAQ
UPS Device Management ... /AP9631CH - UPS Network Management Card ... What UPS Network Management Card ... ... with the AP9631 UPS Network Management Card ... The AP9635 UPS Network Management Card ... to the Symmetra PX 250/500kva and certain Galaxy units also have some ... ... with the AP9631 UPS Network Management Card ... ... with the AP9631 UPS Network Management Card ... ... ap9810) with UPS NMC 2 ( ... ... ap9810) with UPS NMC 2 ( ... ... (ap9810) 8 8 ... ap9810 and AP9631 UPS NMC? ... For firmware v 5 . X . X ... Click on the UPS Tab-> ...
How can I adjust the number of battery packs on a Smart-UPS XL?
Smart- UPS XL products require ... you tell the UPS how many external ... so that the UPS can properly calculate ... Smart- UPS XL ... : Models that begin with SMX are ... Smart- UPS XL models are ... Smart- UPS XL models are ... ... a Smart- UPS performs when it ... the Smart- UPS XL to recognize ... 1. First , EXIT out ... the UPS service must be stopped ... ... go to: Start |Programs | ... ... 2400 baud, 8 data bits, ... 5 . Click on ... ... with an APC UPS or ... (A new unit will display
How do I update the firmware of my SRT series Smart-UPS using the Firmware Upgrade Wizard?
Devices that are *NOT* supported by the Firmware Upgrade Wizard: ... ®, Windows 8 ®, 8 ... ... all but SMC unit : ... menu of the UPS LCD screen select ... down to " UPS Firmware" UPS Model SRT 5 /6KVA ( ... UPS 02.9 SRT 5 /6KVA ( ... UPS 04.1 8 /10kva UPS 04.7 PMU XP1K9NN42RCC UPS 02.3 Upgrading SRT 5 /6KVA units from version 2. x requires updating to ... The first upgrade will bring ... ... upgrading an SRT unit due to a ... ... Upgrading an SRT unit may take up ... ... TURN OFF THE UPS DURING THIS TIME ... You must use the serial cable that is included with your UPS .
Video: What are the different sensitivity settings of a Smart-UPS?
... a Smart- UPS ? Smart- UPS ... The Smart- UPS detects line voltage ... ... default, the UPS reacts to distortions ... plugging into the UPS . ... poor, the UPS may frequently transfer ... ... Battery longevity and service life of the UPS may be conserved ... sensitivity of the UPS , as long ... ... sensitivity, the UPS will transfer at X percent THD. ... Smart- UPS products default to ... ... may allow your UPS to operate online ... time of the UPS . ... Line-Interactive UPS takes to switch ... ... time when the unit is set to ...
PowerChute Network Shutdown lost communications or cannot establish communication with UPS.
... establish communication with UPS . ... .2. X and below. ... PCNS 3. X and above can ... 5 . Verify that the PCNS service is started . If it is already started , try stopping the service and then restarting it again. Instructions for starting and stopping the PCNS service can be found in the Installation guide. ... 8 . If the system is on a different network segment is the system registered with the NMC? ... (See Application note PowerChute Network Shutdown with more than 50 computer connected to one UPS )
Video: How do I configure APC Network Management Card network settings?
... : Environmental Monitoring Unit 1 (AP9312TH ... ... , Environmental Monitoring Units (ap9320, ... ... , Smart- UPS Online (SRT ... ... , Environmental Monitoring Unit , etc) ... ... MAC address that begin with 00 C ... Smart- UPS front panel LCD ... ... Prior 3. x versions allow local ... ... any MAC addresses beginning with 00 C ... ... program, any services using the COM ... ... , the APC UPS service must be stopped ... ... with an APC UPS or accessory. ... ... Connect to the UPS /device serial ... ... Rack Air Removal Unit (acf400, ... ... correct cable, start the terminal emulation ...
How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
... 16 pcs of 100 AH batteries in series(for 5 KVA), the total AH number is 100 AH x 16 pcs= ...
Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
... : Environmental Monitoring Unit 1 (AP9312TH ... ... , Environmental Monitoring Units (ap9320, ... ... , Smart- UPS Online (SRT ... To begin , here is ... ... txt, select UPS debug files ( ... ... v3. X . X , v 5 . X . X , and v6. X . X firmware versions. 1.) Open a command prompt (In a Windows environment: Start > run > "cmd") or other client that supports the FTP protocol. ... 5 .) Type bin ... 8 .) ... 5 .) For config.ini
What does the Force Negotiation setting achieve in the Network Management Card?
... , Environmental Monitoring Units (ap9320, ... ... time for the UPS is calculated differently for a UPS device with outlet ... compared to a UPS without outlet groups ... ... only on the UPS and does not ... For a UPS without outlet groups ... delay for the UPS . For a UPS with outlet groups ... ... available with all UPS devices). Smart UPS Modular devices, with a SKU beginning with SUM, ... ... both types of UPS devices, the ... starts with the NMC ... ... shutdown will affect UPS Outlet Group Power ...


Resultados 1 - 10 de 94

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.