Consultar las preguntas frecuentes



How to install and setup the StruxureOn Gateway
How to install and setup the StruxureOn Gateway Prerequisites A modern well spec’d ... 1. Downloading and installing the Gateway Download and install the Gateway from ... 2. Setting up a proxy server ... the StruxureOn Digital service . ... you are using a proxy server, specify the settings . Click Proxy Settings ... automatically detect proxy settings or configure the settings manually. ... server using these settings . After you install StruxureOn Gateway, use a browser on any ... 3. Discovering devices ... After you have installed the StruxureOn Gateway ... you need to set up which devices you ... ... NetBotz devices with a standard discovery Modbus devices with a Modbus discovery.
Where can I find information for Data Center Operations web services API (Application Programming Interface)?
The StruxureWare Data Center Operation Web Service API is a set of web services that provide access to ... parts of StruxureWare Data Center Operation.
Data Center Expert | How do hardware and software support contracts work?
In the case of a Schneider Electric installation/ configuration service of the systems, the support will begin when the configuration is completed.
Data Center Operation | Unable to pull live data from StruxureWare Data Center Expert?
By examining the DDF that is installed in Data Center Expert we can ... is related to a sensor type being defined correctly or incorrectly.
What are the typical uses for an EcoAisle System
Install ... the ease of service , system flexibility ... running 24 hours a day. ... smooth operation of a data center . ... the temperature of a data center can cause thermal ... ... blade servers become a more relied upon ... in the data center . Capacity planning is yet ... ... aisle / row configuration the cooling system ... ... gained with deploying a containment system enables the cooling capacity to be closely ... Typical data center cooling looks at ... room to adjust capacity . ... changes and send a control signal to ... ... allowing greater cooling capacities without adding more ... Capacity Planning ● Data center expansion ... ● Data center retrofits
Where can I get support for APC and MGE Products?
Assessment Services ... Battery Replacement Services ... Data Center Facility Cooling - Andover Continuum or TAC Vista Data Center Facility Power - PowerLogic ION Enterprise Data Center Software Integration Kits Data Center University ... InfraStruxure for Large Data Centers InfraStruxure for Medium Data Centers ... InfraStruxure for Small Data Centers ... InfraStruxure Type A ... Installation Services ... MGE Service Bypass ... Network Integration Services ... On Site Service ... Operations Capacity ... Power Ready Notebook Cases ... Project Management Services ... Remote Monitoring Services ... Service Bypass Panel Service Plans ... Software Configuration ... Start-Up Service ... Training Services
Why do I need refrigerant traps in my piping?
Data Center Cooling A : A discharge line trap ... ... advised to always install a single trap at ... A : Discharge gas ... ... will reduce compressor capacity and increase compressor ... ... gas velocity to a point where oil ... ... lines reduce system capacity . ... figure 2 for a typical Discharge Line ... ... ok to add a discharge muffler to ... A : Schneider Electric does not require a discharge line muffler ... ... or the District Service Manager discretion. ... Nonetheless, should a discharge muffler be installed it is recommended ... ... easily trapped in a discharge muffler, ... ... Why are we putting in Inverted Traps on ...
Did APC purchase the AirFlow Company?
Data Center Cooling ... 2000 and formed a Network Air Division ... ... We will require a unit model and serial number and a brief description of ... American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... Airflow Company, a leading precision cooling ... ... APC’s stature as a leading, global ... ... and Airflow is a win-win ... ... anticipated to have a growth rate of ... A precision cooling device ... ... systems used in a variety of applications ... ... APC has made a number of strategic ... ) manufacturer Silcon A /S and ... of our global services and consulting organization ... ... Today’s announcement is a continuation of this ... ... globally compatible product set ," said ...
StruxureWare Data Center Expert message stuck retrieving configuration
StruxureWare Data Center Expert message stuck retrieving configuration after pushing a configuration to an SNMP ... StruxureWare Data Center Expert ... APC SNMP device configuration that DCE does not update it's service configuration settings . ... gets stuck in a state of retrieving configuration . ... be selected as a destination device in ... APC SNMP device configuration -> select ... The only way around this at this time is to create a new entry for this device file transfer settings dialog and then reboot the server. This should clear the message and allow future configuration . This issue should be addressed in a future revision.
Setting Up IPMI on StruxureWare Data Center Expert Enterprise
Setting Up IPMI on NetBotz ... StruxureWare Data Center Expert Optional Bios Configurations . ... interface is NOT configured by default on ... ... To enable and configure IPMI administrators must ... IPMI Server Management Configuration Utility". ... access this utility a keyboard and monitor ... ... "IPMI Server Configuration Utility". The following settings should be configured : ... "" is set to "" ... ... "" is set to "" ... ... "" is set to "" ... ... Upon completing the configuration tasks above, ... The utility will save the settings and continue the boot process. ... Check the Dell web site using your Dell service tag to verify hardware version.


Resultados 1 - 10 de 87

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.