Consultar las preguntas frecuentes



Adding External Batteries to an SU, SUM, SURT, SURTA, SURTD or SUA series Smart-UPS XL
... When configuring external batteries with a Smart-UPS XL you must manually tell the UPS how many batteries are connected. Smart-UPS XL ... "SMX" units . ... SMX models have smart batteries which do not ... Smart-UPS XL models do ... communication with the battery packs. ... When configuring external batteries with a Smart-UPS XL you must manually tell the UPS how many batteries are connected. ... SMT and SMX Smart-UPS which use intelligent battery packs and will ... Each external battery pack is configured ... more than 10 battery packs connected.
Why are the battery charge LEDs flashing on a Smart-UPS?
Battery Charge LED Bar ... Smart-UPS , Smart-UPS Online All Smart-UPS models with model ... ... calculated by the Smart-UPS microprocessor) must ... than the low battery signal warning time ... If the UPS calculates the runtime ... than the low battery signal time, the battery charge graph LEDs ... ... Reset the low battery signal time to ... ... for example a Smart-UPS with 15 minutes ... with the low battery signal warning time ... ... , then the battery bar graph LEDs ... ... setting the low battery signal warning time ... and then the UPS Shutdown Parameters submenu ...
Unattended Graceful Shutdown of Cisco Unity Express with an APC UPS
The Smart-UPS will only initiate the shutdown command after its battery capacity has reached less than 5 percent.
PowerChute Network Shutdown 2.2.4 and 4.5G and 5G Smart UPS Behavior
... Management Card 2 UPS application firmware revision apc _hw05_ ... turn off the UPS via PowerChute Network ... the 'On Battery ' and 'Low Battery ' UPS events on certain Smart-UPS models.
What is the expected life of my APC UPS battery?
We do not reccomend using your APC Smart-UPS /Back-UPS as a portable power supply that is repeatedly discharged/recharged ...
Where can I get support for APC and MGE Products?
Smart-UPS Accessories Smart-UPS Battery Systems
How do I recycle APC batteries in the US and Canada?
Product Line: Smart-UPS , Back-UPS
Where can I find MSDS Data, Electrolyte Quantities for InfraStruxure UPSs using APC SYBTU1-PLP batteries
Product line: Symmetra PX, Symmetra LX, Smart-UPS VT, Galaxy 3500, SYBTU1-PLP


Resultados 1 - 10 de 71

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.