Consultar las preguntas frecuentes



Can I change the input power plug on my 120vac Smart-UPS?
... , input, plug, NEMA, 5-15 , L 5 -30, L 5 - 20 , 5 - 20 , ...
NEMA 5-15 receptacle description
Resolution: The NEMA 5-15 receptacle is the most common electrical receptacle in the United
No power output from the Matrix-UPS L14-30 or 5-15 receptacles (mx3000/5000)
... UPS output to the L14-30 receptacle (as well as the NEMA 5-15 receptacles on the Matrix-UPS 3000 model ...
What are the standard output receptacles for the Matrix UPS line?
The Matrix comes standard with (6) 5-15 receptacles, (2) L 6-30 receptacles and (1) ...
SYTF2 for use with Symmetra RM with 208vac Input and Output only
... on the windings of this transformer, he NEMA 5-15 120vac outlets on the rear of the SYTF2 will supply 120 VAC only ...
Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
... creates a traditional 240 v/ 120 v panel where there are 2 legs of 120 v and from hot ... would measure 240 volts .
How do I update the firmware of my SMT, SMX, SMC, or SRT series Smart-UPS?
Devices that are *NOT* supported by the Firmware Upgrade Wizard: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
How do I update the firmware of my SRT series Smart-UPS using the Firmware Upgrade Wizard?
Devices that are *NOT* supported by the Firmware Upgrade Wizard: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
If you need 120 v for your equipment you will still need to use a stepdown transformer.


Resultados 1 - 10 de 66

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.