Consultar las preguntas frecuentes



Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
Please use acac10005 for 300 mm wide applications and acac10010 for 600 mm wide applications.
How to install InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide—acac100010
Issue: InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide —acac100010.
Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?
The installation manual of the Cable Managers for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0 ...
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... Hot Aisle Containment Rack Expansion Bundle Kit ... Install, A Rack Expansion Bundle Kit is a complete set of racks , joining brackets ... A Rack Expansion Bundle Kit is a complete set of racks , joining brackets ... ... store them in a safe location until ... ... side panels from a PDU, UPS ... ... if you are a certified electrician who ... ... correctly install your Rack Expansion Bundle Kit ... ... connected by ground a strap that must ... ... 6×12 mm screws and M ... ... Before attaching new racks to an existing ... (900- mm ) or NetShelter ... (1070- mm ) enclosure.
What's the vertical mounting rail depth for the NetShelter SX cabinets?
... SX cabinets in the proper position for use with rack mountable equipment that has a depth of 29 in (737 mm ).
How is the rackmount U-space of a NetShelter cabinet or rack identified?
1. For any Rackmount device or enclosure - a U or unit of rack space is equivalent to ... or 44.45 mm .
What size bolts are needed to floor mount the NetShelter 4-post rack?
A 5/8" diameter bolt (19 mm ) will fit through the floor ... holes of the NetShelter 4-post rack .
Are 23" mounting rails available for NetShelter SX cabinets?
... : 23" wide mounting rails do not install into 600 mm (24") wide cabinets because the cabinets are not wide enough.
How to remove NetShelter SX rear doors when installed in rows.
When NetShelter SX cabinets are bayed at 600 mm , if the cabinets are not ... remove the right hand rear door from a cabinet.
ACSC1XX Spare Parts List
CABLE ASSY TEMPERATURE SENSORS ( Rack Inlet) ... (2.3 FEET (700 MM ) LONG) ... DC RECTIFIER, 500 WATT, 54VDC, WIDE INPUT, FULL SIGNALS, BLACK ... DIVIDER-' A ' DUCT KIT ACSC 5KW 48ECT BC NKRAFT ... RELAY DPDT 120vac 8 A PC MOUNT


Resultados 1 - 10 de 77

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.