Consultar las preguntas frecuentes



Video: Connect Battery on Back-UPS RS/NS M2 & MS Series
Back-UPS Pro RS/ NS ... All APC UPS systems are shipped with batteries disconnected to comply with US DOT regulations. The UPS will flash the battery icon to indicate a disconnected battery state. ... A severely discharged/damaged battery will also generate the flashing battery alert. The Back-UPS will not be able to recharge or otherwise use a severely discharged battery . ... To connect, disconnect or replace the internal battery , please follow the steps indicated in the video and images below.
Can I change the individual batteries inside of a Smart-UPS replacement battery cartridge?
APC Replacement Battery Cartridges are intended to be replaced as a complete unit.
Used Battery Disposal Options
If you purchased an APC Replacement Battery Cartridge in the ... to return the old battery will be provided with the new Replacement Battery Cartridge.
Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
Why aren't alarms clearing in the BMS (Battery Management System) AP9921X-AP9922 after replacing batteries?
After changing a battery in a string which is monitored by the APC Battery Management System, it is imperative to clear the old baseline ...
How do I recycle APC batteries in the US and Canada?
Please find two options for recycling the old batteries below. They may be recycled locally using call2recycle or though our Replacement Battery Cartridge Recycling Program.
Material Safety Data Sheets (MSDS) or Safety data Sheets (SDS) for Batteries Used in APC UPS Systems
In a few cases, Replacement Battery Cartridges (RBCs) containing High Power Lithium Ion Cell, Phosphate-Based are also used.
Details Returned from APC Devices via Advanced Device Crawlers
Battery Run Time Remaining Battery Replace Indicator
Where can I get support for APC and MGE Products?
Battery Management Battery Replacement Services
What are the basic troubleshooting steps for the APC Back-UPS Pro with Networking bg500 ?
Problem: The Back-UPS is on, the Power On/ Replace Battery LED flashes and the unit emits a constant tone


Resultados 1 - 10 de 83

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.