Consultar las preguntas frecuentes



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units . APC Unit Identification Capacity KW Capacity KW Capacity KW Capacity KW Capacity KW Capacity KW 62 (18T) AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) Capacity KW ... CM 003 ( 1 T) ... -230/ 1 /60 ... =277/ 1 /60 1 -5T ... 1 -3T ... ... -230/ 1 /60 ... =277/ 1 /60 ... CM 15 ( 1 T) ... =208/ 1 /60
3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
Service Level Agreements APC ... ... relates to the service level agreements offered ... 1 Site Inspection Visit 1 set of air ... ... UPS & PDU Advantage Plus : ... _EN_ Advantage Plus 1 Annual PM Visit ... UPS & PDU Advantage Prime: See attached file; ARUO-ACQGSD_R7_EN_ Advantage Prime ... 1 Annual Preventive Maintenance Visit ... UPS & PDU Advantage Ultra: See attached file; ARUO-ACQFVH_R6_EN_ Advantage Ultra ... 1 Annual Preventive Maintenance Visit 1 Set of air filters if applicable ... TSE agent will follow internal protocol to handle the service coverage and necessary actions to process customer requests per SLA.
Where can I get support for APC and MGE Products?
Assessment Services ... Battery Replacement Services ... Environmental Monitoring Unit ... InRoom Direct Expansion ... Installation Services ... Maintenance Bypass Panels ... MGE Service Bypass ... Network Integration Services ... On Site Service ... Planning Tools and Publications ... Power Distribution Units ... PowerChute plus ... Preventive Maintenance Project Management Services ... Remote Monitoring Services ... Service Bypass Panel Service Plans ... Start-Up Service Stationary Power Distribution Units ... Training Services
What are the Dynamic Load ratings and Shipping Load ratings for NetShelter CX cabinets?
Persons planning data centers need ... ... the cabinet, plus installed equipment ( ... These two ratings are different and care should be taken to distinguish between them. ... This is the maximum allowable weight of equipment installed in the cabinet during movement from one location to another within the same data center. ... Example: a customer who wishes to move a cabinet from one row to another in a data center must remove equipment until the weight is equal to (or below) the Dynamic Load Rating before being moved.
How to Install a OROA or A LAC Valve as part of a Flooded Receiver Package
Product line: ACRD1XX, ACRD2XX, ACRP1XX, ACRD5XX, Uniflair DX , Network Air FM, InRoom DX .
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
Devices with an embedded Web/SNMP Card include (but are not limited to): Environmental Monitoring Unit 1 (AP9312TH)
What do I gain with a Unity Output Power Factor (kW=kVA)?
... Power Factor ( kW =kVA) ... ... Power Factor ( kW =kVA) ... The advantage of unity power ... Some APC 3-phase UPS products as well as newer single phase products(SRT6K) have an output rating of kW =kVA or Unity Power Factor. While the more traditional double conversion units have output ratings of kW =0.8kva. ... https://www.apc.com/salestools/SADE-5TNQYL/SADE-5TNQYL_R 1 _EN.pdf
What are the operational conditions for an InRoom (Stulz) Unit
... conditions for an InRoom (Stulz) Unit . The InRoom precision air conditioning units operate within the ... ... +/- 1 % ... between the cooling unit and the air ... ... and the cooling unit : 5 m ... below the cooling unit ... evaporator capacity ( DX ): 24 ... Cooling fluid ( DX ): 30% Glycol ... Downflow units with an external static pressure: 20 Pa (0.08 in w g) Upflow units with an external static pressure: 50 Pa (0.20 in w g)
Stulz Tech Data Manual
ACPDX21-86, acpcw40-150, Tech Data Manual, Stulz, Chilled Water, Dx , Inroom
Network Air FM unit spare parts list
... Network Air FM unit . Always ADAPTER ROTO 1 1 /4" ... ADAPTER ROTO 1 "-14R ... ... CAT5 for EXP unit ... - MKC- 1 ... ASSY FM 35 KW DX ... ASSY FM 40 KW DX ... ASSY FM 50 KW DX ... compressor [K 1 & K2 ... ... DF 5/ Unit 756 X 325 ... ... DF 5/ Unit 756 X 325 ... ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ...


Resultados 1 - 10 de 77

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.