Browse FAQs



Please explain Suction Pressure Compensation for the NetworkAIR FM.
Issue: Please explain Suction Pressure Compensation for the NetworkAIR FM.
Whether to install a suction line drier or liquid line drier
Issue: Whether to install a suction line drier or liquid line drier
NetworkAIR FM Secondary Compressor Lock Out
NetworkAIR FM Secondary Compressor will not Turn On If the suction pressure on the ... stop to avoid suction pressues that can form ice on the coil resulting in undesired down time..
How does the ACSC calculate capacity in realtime?
In Spot-Discrete mode the unit measures the refrigerant suction and discharge pressures to calculate the compressor performance; then subtracts the losses from ...
Are there any 600mm units that have return air temperature limits for warranty purposes?
... This temperature is driven from maximum limits of accessory and support products and to maintain suction gas temperatures within acceptable range on the DX units ...
Where should the TEV External Equalizer be installed and where should the TEV bulb be located?
The purpose of the external equalizer is to sense the pressure in the suction line AT THE BULB LOCATION and transmit it to the TEV ...
What is the purpose of Refrigerant Piping Insulation?
Internal to an air conditioner suction lines temps are about (40°F ... is below the dewpoint of the coil/ suction lines.
InRow: What is capacity regulation?
As the suction pressure drops the valve will start to feed discharge gas into the evaporator coil raising the overall suction pressure.
Pressure and Temperature Symptoms Chart
and Temperature Symptoms Chart: Symptoms Exhibited * Condition Solutions Suction


Results 1 - 10 of 17

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.