Browse FAQs



Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products
Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products
Galaxy VX; How to configure the Network Communications options
How to configure the Network Communications options for Galaxy VX ... Galaxy VX - all ... How to set up network communications for the UPS ... The network can be configured for the display and for the cards in Smart Slot 1 and ... Smart Slot 1
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
... ) circuit to Galaxy VX ? Galaxy VX ... ) circuit to Galaxy VX ? ... A35JB8_R 1 _EN. ... When the UPS is EPO'd, ... There is also an option in the UPS Tuner ( ... software) to have the UPS go to static bypass on EPO (default setting is no). ... Tripping of the upstream breaker could be a code requirement, typically if UPS is located in the data center. ... Note; in parallel systems, only the UPS in which the EPO is activated is affected; remaining UPS will still be powered.
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM. ... Galaxy VX , Galaxy VM ... The display of the Galaxy VX and VM is part of the NMC and has been disabled. ... Use the console cable supplied with UPS ... Serial port setting: for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control. ... Assuming the UPS is connected to the customer network and is granted an DHCP IP address.
Serial communications between Smart-UPS VTs, Galaxy 3500, and Symmetra PX with IBM AS/400, i Series
... configure Smart- UPS VTs, Galaxy 3500, and ... ... 3-phase UPS systems. FA159551 K -Base. ... ... to set a UPS to ‘never ... *Available UPS Signalling Options for ... ... 3-phase UPS ) ... a Smart- UPS VT, Galaxy 3500, Symmetra ... -phase supported UPS , please follow ... ... SmartSlot of the UPS . If the UPS has two or ... ... needed and your UPS only has one SmartSlot, attach ... port of the UPS and install the ... *Available UPS Signalling Options for IBM AS/400 & IBMi (IBM Power Systems) can be found in
Where do I find an Operation Manual for Galaxy VX Series UPS?
Issue: Operation Manual for Galaxy VX Series


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.