Browse FAQs



PowerChute Business Edition unsuccessfully installing on Linux after multiple installations on the server
Follow the steps below to rebuild the rpm database and successfully install PowerChute: NOTE: The above command will differ for 32 - bit and 64-but Linux operating systems.
Why can I not install PowerChute Business Edition on RHEL 5.11?
Issue: When installing PowerChute Business Edition on RHEL 5.11, the following error message is seen, “RSA/SHA1 signature:BAD, RPM cannot be installed” and the installation is unsuccessful. This happens because RPM signing keys are not supported for RHEL 5.11. Product: PowerChute Business Edition v9.5 and above Environment: RHEL 5.11 Solution: For v9.5 Execute the following command: rpm --nosignature -i pbeagent-9.5.0-301.XX.rpm NOTE: The above command will differ for 32 - bit and 64- bit Linux operating systems. 32 - bit Linux: rpm pbeagent-9.5.0-301.i386.rpm 64- bit Linux: rpm pbeagent-9.5.0-301.x86_64.rpm For v10 Execute the following command: rpm --nosignature -i pbeagent-10.0.0-301-EN.x86_64.rpm NOTE: The above command will differ based on your locale. English: rpm pbeagent-10.0.0-301-EN.x86_64.rpm Chinese: rpm pbeagent-10.0.0-301-CN.x86_64.rpm This command tells RPM to ignore the signature when installing PowerChute Business Edition and will treat the RPM as unsigned. NOTE: You will not be able to verify the RPM package on RHEL 5.11. However, this is the case for previous versions of PowerChute that were unsigned. To uninstall PowerChute Business Edition on RHEL 5.11, execute the following command: rpm --nosignature -e pbeagent PCBE
PowerChute Business Edition – Simple Signaling with Interface Expander 2 card shutdown delay
PowerChute Business Edition v9.5 and above ... 12 minutes ( 32 minutes in total) ... : This issue is specific to Type B UPS devices only
PowerChute Personal Edition v3.X Error Code 2738 – Unable to install the software.
Follow the below steps to register Vbscript.dll: To do this on a 32 bit system :
Manual Removal of PowerChute Personal Edition on Windows Systems
1. From the installation directory in Explorer (e.g. 32 Bit
Schneider Electric's Technical Support Policy for Older Versions of PowerChute Software
PowerChute Network Shutdown ( ... PowerChute Business Edition (PCBE) ... PowerChute Personal Edition (PCPE) ... PowerChute Plus (PC ... ... shipping version of PowerChute Network Shutdown is ... support is continuing for PCNS 4.2 for 32 bit systems , and PCNS v4.3 for 64- bit systems . ... The current shipping version of PowerChute Business Edition is 10.0.1 ... support is continuing for PCBE 9.5 for 32 bit systems . The current shipping version of PowerChute personal Edition is 3.1 It was release June 2019 PowerChute Plus was discontinued March 2007


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.