Browse FAQs



Can a 3rd party UPS be installed in the ar106v or ar106vi?
Cause: The NetShelter WX 6U Vertical cabinets have a mounting bracket for a 2 U UPS.
Are the new 6U, 9U and 12U NetShelter cabinets hinged in the rear, like ar100 & ar100hd?
Customers inquire if the newer 6U , 9 U and 12U wall mount cabinets are hinged in the rear. ... NetShelter WX ... The 13U NetShelter WX cabinets are hinged in the rear. ... The new 6U , 9 U and 12U NetShelter WX cabinets (ar106, ar109, AR112) are not ... Only the NetShelter WX ar100 and ar100hd are hinged in the rear,
In the NetShelter WX 6U Vertical cabinet, can the 2U UPS Mounting Bracket also be used on a 1U or 3U Smart-UPS?
Issue: It is unknown whether a 1 U ot 3 U Smart-UPS can use the 2 U mounting rail.
Does the NetShelter WX castor kit AR8359 fit onto the ar106, ar109 or AR112.
Issue: There doesn't appear to be a castor kit for the 6U , 9 U or 12U NetShelter WX cabinets.


Results 1 - 7 of 7

  • 1

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.