Browse FAQs



Can I mix old and new batteries in a Smart-UPS?
When replacing the battery cartridges in this APC Smart-UPS ... system, the two battery modules for the ... and the four battery modules for the external battery pack should be ...
Video: How to Select the Correct Replacement Battery Cartridge (RBC) for your UPS
... The UPS indicates battery replacement is required or ... Battery replacement is part of ... UPS Replacement Battery Selector ... determine the correct Replacement Battery Cartridge to purchase for your APC UPS and to ... ... on www. apc .com. The first two numbers in the ... ... you need a replacement battery cartridge . A battery will typically last ... UPS Replacement Battery Selector ... , go to APC's convenient, easy ... ... or purchasing a replacement battery cartridge (RBC) ... ... you purchase a Replacement Battery cartridge (RBC) ... units contain multiple batteries inside the UPS ... ... contain all the batteries you will need ...
Can I change the individual batteries inside of a Smart-UPS replacement battery cartridge?
APC Replacement Battery Cartridges are intended to be replaced as a complete unit.
Used Battery Disposal Options
If you purchased an APC Replacement Battery Cartridge in the U ... return the old battery will be provided with the new Replacement Battery Cartridge .
Why are the battery charge LEDs flashing on a Smart-UPS?
Battery Charge LED Bar ... ... be AT LEAST two minutes more than the low battery signal warning time ... ... being less than 2 minutes more than the low battery signal time, the battery charge graph LEDs ... ... Reset the low battery signal time to ... ... with the low battery signal warning time ... ... , then the battery bar graph LEDs ... ... setting the low battery signal warning time ... Two minutes is the ... ... , the low battery signal time is ... Option 2 : UPS battery ... /www. apc .com/ ... ... the load or replace the battery . ... , yet the batteries are consumable items ...
Video: APC AV S Type Power Conditioner w/ Battery Back-up - Battery Replacement Procedure
Resolution: The following video details the process for removing and reinstalling the internal Replacement Battery Cartridge .
How do I recycle APC batteries in the US and Canada?
Pack the used battery in the packaging from the replacement battery cartridge and affix the return label.
Material Safety Data Sheets (MSDS) or Safety data Sheets (SDS) for Batteries Used in APC UPS Systems
In a few cases, Replacement Battery Cartridges (RBCs) containing High Power Lithium Ion Cell, Phosphate-Based are also used.
Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
Video: Why might my APC Back-UPS Product be beeping?
... 15 seconds and will yield one of 2 results: If the Replace Battery LED stays lit ... test) the battery should be replaced .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.