Technical FAQs

Ask a Question

Data Center Operation | How to download the desktop client?

Issue:
Process for downloading the Data Center Operation desktop client.

Product Line:
StruxureWare Data Center Operation (DCO)

Environment:
StruxureWare Data Center Operation (DCO)

Resolution:

Data Center Operation 8.X
1) Log into the web interface.
2) Click on the round icon in the upper-right with your user initials in it.
3) Click on Download.
4) Click on Download next to the download option that you require.
5) Select your Operating System.

NOTE: Starting with DCO version 8.2.7, the desktop client is not contained within the ISO and is downloaded from an external site when you click on the operating system version.  If you experience issues with the download, please ensure that your computer has internet access and that the download is not being block on your network.


Data Center Operation 7.X and earlier:

1) Navigate to the DCO web interface.
2) Select the option to download the Desktop Client.
Was this helpful?
What can we do to improve the information ?