Issue:
How do I find the Java version the StruxureWare Data Center Expert desktop client is using?
Product line:
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
Environment:
StruxureWare Data Center Expert (all versions)
Resolution:
The Java version that the DCE Desktop Client uses can be found within the related Program Files folder:
1) Open Windows Explorer and navigate to your main disk driver (usually C:).
2) Open the installation directory, which will be in one of two places (default):
- Version 7.7.0 and prior: C:\Program Files (x86)\StruxureWare Data Center Expert X.X.X
- Version 7.7.1 and later: C:\Program Files\StruxureWare Data Center Expert X.X.X
3) Navigate into the dcexpert folder and then into the jre folder.
4) Open the release file in a text editor such as notepad.
5) The Java version is displayed on the first line of the document.
NOTE: The Java version can not be updated manually. If a Java update is necessary, it will be included in future DCE versions of the software.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.