Browse FAQs

Does the NetBotz Leak Rope Sensor NBES0308 detect leak location / zone?

Published date: 29 May 2019

Issue:
NetBotz Leak Rope sensor does not detect zone.

Product Line:
NetBotz

Environment:
NetBotz leak Rope NBES0308 / NBES0309

Cause:
Leak rope integration into Botzware does not detect the location or zone along the cable where the leak is detected.

Resolution:
The Leak Rope sensor and extension acts like a dry contact. It either detects conductivity or does not. The NetBotz appliance has no code in it to detect where on the cable or it's extensions that it has detected a leak.

If it is critical to know where exactly a leak has been detected, it is suggested that you use spot leak sensors instead of a rope leak.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.