Browse FAQs

NetBotz 750 state sensor appears as "Disconnected" after reboot of the appliance.

Published date: 11 April 2019

Issue:

NetBotz 750 state sensor appears as "Disconnected" after reboot.

Product Line:

NetBotz

Environment:

NBRK0750
Version 5.1.0 firmware
State Sensors

Cause:

After rebooting a NetBotz 750 running 5.1.0 firmware, the connected state sensors (dry contact, leak, vibration, etc.) may appear in the NetBotz UI as "Disconnected".

Resolution:

Disconnect and reconnect each sensor. This allows the appliance to detect the sensors again.
This will be resolved in the next release of the firmware.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.