Browse FAQs

Video: Configuring output relays/input contacts on a Galaxy VM

Published date: 07 May 2018

Issue:
Configuring Input Contacts & Output Relays on Galaxy VM UPS Display
 
Product line:
Galaxy VM
 
Environment:
All Product models, all serial numbers
 
Cause:
Configuring output relays/input contacts on a Galaxy VM

Resolution: 
Follow the steps for configuring Output relays and Input contacts on a Galaxy VM.
 
Input Contacts:
Battery Charging
Alarm Configuration
 
Output Relays:
Communicate Status conditions with external Monitoring System
 
Start from the Home screen
Select ‘configuration’
Select ‘Output Relay’ or ‘Input Contacts’
 
Configure the setting as meets your needs.
Select "OK" to save your settings

The following video demonstrates this procedure:


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.